MCUXpresso Supported Devices Table - Lacks LPC51U68

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Supported Devices Table - Lacks LPC51U68

Jump to solution
1,903 Views
larsen
Contributor III

As of April 10. 2019 on this webpage: MCUXpresso Supported Devices Table (dated March 28 2019)

the downloaded excel sheet has no mention of LPC51U68 support - yet it is supported with an SDK for MCUXpresso.

0 Kudos
Reply
1 Solution
1,693 Views
CJarvis
NXP Employee
NXP Employee

That specific thread is locked for comments.  I have corrected the issue and added the LPC51U68 to the supported table.

View solution in original post

0 Kudos
Reply
5 Replies
1,693 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

I would suggest you add comment to that thread. thus the author can know this.

Have a nice day,

Jun Zhang

0 Kudos
Reply
1,693 Views
larsen
Contributor III

Yes you are right. I would have done that if I could, but there is no way for me to reply to this thread - strange as it may seem.

0 Kudos
Reply
1,693 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Thank you for letting us know.

I just checked this doc LPC51U68 is there. see below. can you please check it again?

pastedImage_5.png

 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,693 Views
larsen
Contributor III

Thanks Jun,

i think it got corrected in the meantime. But bottom line - Now its correct.

br henning

0 Kudos
Reply
1,694 Views
CJarvis
NXP Employee
NXP Employee

That specific thread is locked for comments.  I have corrected the issue and added the LPC51U68 to the supported table.

0 Kudos
Reply