Hello NXP community,
I have powered my T2080 QDS board as usual and suddenly the U-Boot output was like in the screenshot below. Can anyone provide me with a solution on how to get rid of this error? Currently I am stuck at this point not knowing how to move on.
Hello crashbuzz,
First please make sure that you are using the original DDR provided in T2080QDS.
Please use the default clock(Core/Platform/DDR = 1800MHz/600MHz/1866MT/s) configuration on the target board.
Please configure your target board to the default switch settings.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello yipingwang
thank you for the answer. Can you tell me which one is the "original DDR provided in T2080QDS". Maybe I have the wrong one.
Regards