Can I change NFC detecting range on CLRC663 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I change NFC detecting range on CLRC663 ?

821 Views
cjujh
Contributor I

Hello.

I've been making NFC module using CLRC663 IC on CLEV6630B v2.0 Board nowadays.

I'd wanted to change the NFC detecting range by only use software setting.

So I'd checked datasheet and modified below register and 0x28 and 0x2A registers too.

pastedImage_3.png

But, it was operated same range.

Is it possible to change the range? How can I do that?

Thank you.

Labels (2)
0 Kudos
Reply
1 Reply

655 Views
Kan_Li
NXP TechSupport
NXP TechSupport

I am sorry, but the operating range depends on the antenna size, please refer to the following for details.

pastedImage_1.png

You may refer to NFC Antenna Design 1: Which Antenna for what purpos|NXP  for more details.

Hope that helps,


Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply