PF1510 driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF1510 driver

Jump to solution
2,229 Views
norman_stetter
Contributor I

Hello,

is the pf1550 driver from the imx_4.9.88_2.0.0_ga  kernel compatible with the pf1510?

I also checked imx_4.14.78_1.0.0_ga, which doesn't have a driver for pf1510 either.

My processor is a IMX6ULL (MCIMX6Y2CVM08AB)

Regards,

Norman

Labels (1)
0 Kudos
Reply
1 Solution
1,952 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Norman,

 

PF1550 and PF1510 are similar to each other with some specific features of difference:

PF1510 specific features: 1.5 A front-end LDO

PF1550 specific features: Linear 1 A Li+ Battery Charger 

 

The PF1510 is same as PF1550 except for the charger function, we removed the charging function for the PF1510.

 

If you are not planning to use these specific features, then the PF1550 driver should be compatible for the PF1510.

 

These PMICs share the same address and register map (except for the special features), so, PF1550 driver can be used for PF1510, just ignore charger related operations.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,953 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Norman,

 

PF1550 and PF1510 are similar to each other with some specific features of difference:

PF1510 specific features: 1.5 A front-end LDO

PF1550 specific features: Linear 1 A Li+ Battery Charger 

 

The PF1510 is same as PF1550 except for the charger function, we removed the charging function for the PF1510.

 

If you are not planning to use these specific features, then the PF1550 driver should be compatible for the PF1510.

 

These PMICs share the same address and register map (except for the special features), so, PF1550 driver can be used for PF1510, just ignore charger related operations.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply