DDR Stress Test Tool on the iMX6ULEVK via JTAG again.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Test Tool on the iMX6ULEVK via JTAG again.

4,161 Views
titggtu
Contributor II

I'd like to run the DDR Stress Test Tool on the iMX6ULEVK via JTAG using Segger JLink.

I modified the EVK hardware (removed R1407, R1431 to R1434 and added R1912 and R1914 to R1916).

I initialize a connection with JLink.exe and the commands:

device MCIMX6Y2 (MPU on my EVK MCIMX6Y2DVM09AA)

connect

Type "connect" to establish a target connection, '?' for help

J-Link>connect

Please specify device / core. <Default>: MCIMX6Y2

Type '?' for selection dialog

Device>

Please specify target interface:

  1. J) JTAG (Default)
  2. S) SWD
  3. T) cJTAG

TIF>j

Device position in JTAG chain (IRPre,DRPre) <Default>: -1,-1 => Auto-detect

JTAGConf>

Specify target interface speed [kHz]. <Default>: 4000 kHz

Speed>

Device "MCIMX6Y2" selected.

 

Connecting to target via JTAG

Executing J-Link script file function: ConfigTargetSettings()

_____________J-Link script: Setting up AP map__________________

TotalIRLen = 13, IRPrint = 0x0101

*************************

WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet = 2)

**************************

JTAG chain detection found 3 devices:

 #0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP

 #1 Id: 0x00000001, IRLen: 05, Unknown device

 #2 Id: 0x088C101D, IRLen: 04, JTAG-DP

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[1]: APB-AP (IDR: Not set)

Using preconfigured AP[1] as APB-AP

AP[1]: APB-AP found

ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-001BB961 TMC

ROMTbl[0][1]: CompAddr: 80002000 CID: B105900D, PID:04-004BB906 CTI

ROMTbl[0][2]: CompAddr: 80003000 CID: B105900D, PID:04-004BB912 TPIU

ROMTbl[0][3]: CompAddr: 80004000 CID: B105F00D, PID:04-001BB101 TSG

ROMTbl[0][4]: CompAddr: 80020000 CID: B105100D, PID:04-000BB4A7 ROM Table

ROMTbl[1][0]: CompAddr: 80030000 CID: B105900D, PID:04-005BBC07 Cortex-A7

Found Cortex-A7 r0p5

6 code breakpoints, 4 data breakpoints

Debug architecture ARMv7.1

Data endian: little

Main ID register: 0x410FC075

I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way

D-Cache L1: 32 KB, 128 Sets, 64 Bytes/Line, 4-Way

Unified-Cache L2: 128 KB, 256 Sets, 64 Bytes/Line, 8-Way

System control register:

  Instruction endian: little

  Level-1 instruction cache enabled

  Level-1 data cache disabled

  MMU disabled

  Branch prediction enabled

Memory access: CPU temp. halted: https://wiki.segger.com/Memory_accesses#Legacy_stop_mode

Clock Init Done

DDR Init Done

Memory zones:

  [0]: Default (Default access mode)

  [1]: AHB-AP (AP0) (DMA like acc. in AP0 addr. space)

  [2]: APB-AP (AP1) (DMA like acc. in AP1 addr. space)

Cortex-A7 identified.

J-Link>

 

J-Link script initializes CLK and DDR, in accordance with the example script provided in EVK_IMX6ULL_DDR3L_400MHz_512MB_16bit_V1.2.ink.

Then I load the ddr-test-uboot-jtag-mx6ull.bin image using the loadbin command at address 0x00907000.

I connected the COM1 port to the computer and made sure that it was working by sending data to the UART Transmitter Register (UART1_UTXD) register.

 

Next, I have to run the downloaded image for execution.

First question: How to do it right?

The second question is: Should MUU and Level-1 data cache be enabled?

In my case they are off.

«System control register:

  Instruction endian: little

  Level-1 instruction cache enabled

  Level-1 data cache disabled

  MMU disabled

  Branch prediction enabled»

But boot eFUSE   BT_MMU_DISABLE – installed to 0.

J-Link script initializes CLK and DDR attached.

Thanks, Alexey.

Labels (2)
4 Replies

3,662 Views
titggtu
Contributor II

I found a solution to my problem. To run the test, it is necessary to reset the processor correctly.

See ARM Architecture Reference Manual section A2.6.2 Reset:

A2.6.2 Reset
When the Reset input is asserted on the processor, the ARM processor immediately stops execution of the
current instruction. When Reset is de-asserted, the following actions are performed:

 

 

R14_svc

= UNPREDICTABLE value

 

SPSR_svc = UNPREDICTABLE value
CPSR[4:0] = 0b10011

/* Enter Supervisor mode */
/* Execute in ARM state */
/* Disable fast interrupts */
/* Disable normal interrupts */
/* Disable Imprecise Aborts (v6 only) */

 

CPSR[5]
CPSR[6]
CPSR[7]
CPSR[8]

= 0
= 1
= 1
= 1

 

 

 

Next, I provide a log of the connection with the i.MX 6ULL EVK debug board.

SEGGER J-Link Commander V6.40 (Compiled Oct 26 2018 15:06:29)

DLL version V6.40, compiled Oct 26 2018 15:06:02

 

Connecting to J-Link via USB...O.K.

Firmware: J-Link V10 compiled Oct 26 2018 12:04:17

Hardware version: V10.10

S/N: XXXXXXXX

License(s): FlashBP, GDB

OEM: SEGGER

VTref=3.317V

 

Type "connect" to establish a target connection, '?' for help

J-Link>connect

Please specify device / core. <Default>: MCIMX6Y2

Type '?' for selection dialog

Device>

Please specify target interface:

  1. J) JTAG (Default)
  2. S) SWD
  3. T) cJTAG

TIF>

Device position in JTAG chain (IRPre,DRPre) <Default>: -1,-1 => Auto-detect

JTAGConf>

Specify target interface speed [kHz]. <Default>: 4000 kHz

Speed>

Device "MCIMX6Y2" selected.

Connecting to target via JTAG

Executing J-Link script file function: ConfigTargetSettings()

_____________J-Link script: Setting up AP map_____________

TotalIRLen = 13, IRPrint = 0x0101

**************************

WARNING: At least one of the connected devices is not JTAG compliant (IEEE Std 1149.1, 7.1.1.d, IR-cells). (NumDevices = 3, NumBitsSet = 2)

**************************

JTAG chain detection found 3 devices:

 #0 Id: 0x5BA00477, IRLen: 04, CoreSight JTAG-DP

 #1 Id: 0x00000001, IRLen: 05, Unknown device

 #2 Id: 0x088C101D, IRLen: 04, JTAG-DP

AP map detection skipped. Manually configured AP map found.

AP[0]: AHB-AP (IDR: Not set)

AP[1]: APB-AP (IDR: Not set)

Using preconfigured AP[1] as APB-AP

AP[1]: APB-AP found

ROMTbl[0][0]: CompAddr: 80001000 CID: B105900D, PID:04-001BB961 TMC

ROMTbl[0][1]: CompAddr: 80002000 CID: B105900D, PID:04-004BB906 CTI

ROMTbl[0][2]: CompAddr: 80003000 CID: B105900D, PID:04-004BB912 TPIU

ROMTbl[0][3]: CompAddr: 80004000 CID: B105F00D, PID:04-001BB101 TSG

ROMTbl[0][4]: CompAddr: 80020000 CID: B105100D, PID:04-000BB4A7 ROM Table

ROMTbl[1][0]: CompAddr: 80030000 CID: B105900D, PID:04-005BBC07 Cortex-A7

Found Cortex-A7 r0p5

6 code breakpoints, 4 data breakpoints

Debug architecture ARMv7.1

Data endian: little

Main ID register: 0x410FC075

I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way

D-Cache L1: 32 KB, 128 Sets, 64 Bytes/Line, 4-Way

Unified-Cache L2: 128 KB, 256 Sets, 64 Bytes/Line, 8-Way

System control register:

  Instruction endian: little

  Level-1 instruction cache enabled

  Level-1 data cache disabled

  MMU disabled

  Branch prediction enabled

Memory access: CPU temp. halted: https://wiki.segger.com/Memory_accesses#Stop_mode

/*Run the script and initialize the CLK and DDR3 */

Clock Init Done

DDR Init Done

Memory zones:

  [0]: Default (Default access mode)

  [1]: AHB-AP (AP0) (DMA like acc. in AP0 addr. space)

  [2]: APB-AP (AP1) (DMA like acc. in AP1 addr. space)

Cortex-A7 identified.

J-Link>h

PC: (R15) = 0000883C, CPSR = 400001F3 (SVC mode, THUMB FIQ dis. IRQ dis.)

Current:

     R0 =00002040, R1 =00900A30, R2 =10000000, R3 =00000800

     R4 =00000000, R5 =00000002, R6 =00900BA4, R7 =02020000

     R8 =00008840, R9 =00008840, R10=021E8000, R11=0001C200, R12=000100A1

     R13=00020200, R14=020E0014, SPSR=0091FF64

USR: R8 =021E8000, R9 =0001C200, R10=000100A1, R11=00020200, R12=020E0014

     R13=B08071EC, R14=9410365C

FIQ: R8 =145A4BAC, R9 =13E07390, R10=28E18AA4, R11=82091972, R12=94128C58

     R13=34957FE8, R14=67C0680F, SPSR=8101005D

IRQ: R13=2D235DD0, R14=F46B68C4, SPSR=A0030921

SVC: R13=0091FF64, R14=000085E5, SPSR=000001D3

ABT: R13=3B0D2E20, R14=100340EC, SPSR=C1000438

UND: R13=B30D98D8, R14=AE1A2C3B, SPSR=22040E62

/*Reset the CPCR register in accordance with the documentation.*/

J-Link>wreg CPSR 0x000001d3

CPSR = 0x000001D3

J-Link>regs

PC: (R15) = 0000883C, CPSR = 000001D3 (SVC mode, ARM FIQ dis. IRQ dis.)

Current:

     R0 =00002040, R1 =00900A30, R2 =10000000, R3 =00000800

     R4 =00000000, R5 =00000002, R6 =00900BA4, R7 =02020000

     R8 =00008840, R9 =00008840, R10=021E8000, R11=0001C200, R12=000100A1

     R13=00020200, R14=020E0014, SPSR=0091FF64

USR: R8 =021E8000, R9 =0001C200, R10=000100A1, R11=00020200, R12=020E0014

     R13=B08071EC, R14=9410365C

FIQ: R8 =145A4BAC, R9 =13E07390, R10=28E18AA4, R11=82091972, R12=94128C58

     R13=34957FE8, R14=67C0680F, SPSR=8101005D

IRQ: R13=2D235DD0, R14=F46B68C4, SPSR=A0030921

SVC: R13=0091FF64, R14=000085E5, SPSR=000001D3

ABT: R13=3B0D2E20, R14=100340EC, SPSR=C1000438

UND: R13=B30D98D8, R14=AE1A2C3B, SPSR=22040E62

/*load the bin file into memory at 0x00907000*/

J-Link>loadbin ddr-test-uboot-jtag-mx6ull.bin 0x00907000

Downloading file [ddr-test-uboot-jtag-mx6ull.bin]...

O.K.

/*Install a PC to this address and start the processor*/

J-Link>setPC 0x00907000

J-Link>g

J-Link>

After starting the processor, a memory test is started in the console.

DDR_sterss_test.PNG

I think the problem is solved.

3,662 Views
titggtu
Contributor II

Hello,

Thanks for the help I will try.

I use version V6.40 of the J-Link software.
i.MX6/7 DDR Stress Test Tool V3.00 behaves exactly the same as V2.92.
Are there any other solutions to the problem?

0 Kudos
Reply

3,662 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the recent DDR test version

https://community.nxp.com/docs/DOC-105652 

Regards,

Yuri.

0 Kudos
Reply

3,662 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Following forum states about issues with i.MX 6UL, that was resolved in

in version 6.14c of the SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace 

[SOLVED] I.MX6UL support in segger j-link probe - J-Link/Flasher related - SEGGER - Forum 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply