codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior

643 Views
edison_wu76
Contributor I

Hi  sir,

I am the beginner.

I bough the DEVKIT-S12XE demo board.

and download the "DEVKIT-S12XE-QSP" from the NXP website.

I build to open the "Lab1_KB_S12XE" project by IDE codewarroir 5.9.0, but it's failed.

the error massage below the photo.

thanks.

Edison.

unnamed.png

unnamed (1).png

0 Kudos
Reply
1 Reply

545 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello edison wu,

From the error message, it seems connect board failed .

Please add a 12V power on J9 , also first create a simple new project , build, download to have a try.

pastedImage_1.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------