Does the MCIMX6SLL-EVK support SDIO UHS-I mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the MCIMX6SLL-EVK support SDIO UHS-I mode

Jump to solution
860 Views
ko-hey
Senior Contributor II

Hi all

 

Does the MCIMX6SLL-EVK support SDIO UHS-I mode ?

 

I know that the i.MX6SLL supports UHS-I compliant.

Can we support SDIO UHS-I mode with the same circuit configuration as the MCIMX6SLL-EVK ?

 

Do I need a 1.8 V / 3.3 V switching device based on the SDx_VSELECT signal externally ?

 

Ko-hey

 

Labels (4)
1 Solution
711 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

there is no need for external 1.8 V / 3.3 V switching since i.MX6SLL (as i.MX6SL) has pad dual voltage

capability : NVCC_3V3, NVCC_1V8. In linux dts there is option for sd high frequency pad settings:

pinctrl_usdhc1_100mhz: usdhc1grp_100mhz
pinctrl_usdhc1_200mhz: usdhc1grp_200mhz

linux/arch/arm/boot/dts/imx6sll-evk.dts

imx6sll-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
712 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

there is no need for external 1.8 V / 3.3 V switching since i.MX6SLL (as i.MX6SL) has pad dual voltage

capability : NVCC_3V3, NVCC_1V8. In linux dts there is option for sd high frequency pad settings:

pinctrl_usdhc1_100mhz: usdhc1grp_100mhz
pinctrl_usdhc1_200mhz: usdhc1grp_200mhz

linux/arch/arm/boot/dts/imx6sll-evk.dts

imx6sll-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply