The Allegro LAY-29615_B2.brd file in the X-MCIMX8M-EVK_RevB3_DESIGNFILES package will not import into Altium.
Can I get a Allegro text based ALG file to import into Altium?
It looks like the latest version is Rev B4, but the schematics that you can download are Rev B3.
I have not seen any files yet?
I do not have the text ALG file that is needed. The files online are only BRD binaries.
The BRD files may be able to be saved as an order version or text version which might work, but I know the text version of the ALG file works.
Anyone with Allegro should be able to load the files and save them in the other format.
Hello,
the file was sent via e-mail.
Regards,
Yuri.
Hello,
I have sent You message about Allegro files of the design files, located on the Web.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!