lpc 43s70 HSADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc 43s70 HSADC

517 Views
HeMyFAE
NXP Employee
NXP Employee

DEar LPC,

 

For the LPC43S70 HSADC I have a following questions for you.

 

1)      We are planning on using the 12 Bit High Speed ADC converter at 60 MHz data rate for high speed data sampling.  Do you have any application notes or advice on the best PCB layout techniques for minimum noise / optimum performance?

2)      For the same ADC converter, do you also have any application notes or advice on the best differential driving technique to drive into the LPC43S70 ADC Converter?

Regards,

hy

0 Kudos
Reply
1 Reply

408 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Hy,

Please find LPC MCU ADC design guidelines from TN00009 document.

There also provides PCB layout guidlines for NXP MCU in BGA packages at AN10778.

Besides of above documents, you also could get some design reference at LPC43xx evaluation board below:

OM13088: LPCXpresso4367 Development Board

OM13031: Hitex LPC4350 Evaluation board

OM13040: Keil MCB4357 Evaluation Board and Internet Radio Solution

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply