Hi community,
I had designed an application with QT5.4.
And I used Qquickwidget and Qmediaplayer to complete my functionality.
I am getting start at using Yocto Project 2.0 released by freescale.
And I wondering which backend and image is suitable for me to use.
According to the reference, it has some images that I can choose to build related to below picture.
I suppose that these are options which rootfs I want to build.
And below picture is the option to choose which backend that you want.
Here is my question.
which backend and rootfs do I need to build for running my application?
Is there any suggestions?
Additional question, can anyone teach what is the difference between wayland and X11?
Although I have a lot of research on the internet, I still cannot understand what are these two suppose to do.
And still cannot understand what is the difference between -platform wayland and -platform eglfs.
I would be grateful that anyone who can teach me.
Thanks in advanced!