Hi,
I'm using i.MX8M custom board.
Here MFG tool is failing in below place. Using Type C as OTG.
The available udc:
/sys/class/udc/38100000.dwc3
[ 5.940293] Mass Storage Function, version: 2009/09/11
[ 5.945456] LUN: removable file: (no medium)
MFG tool will use 1st udc:38100000.dwc3
/linuxrc: line 53: echo: write error: Device or resource busy
Starting UTP
uuc 0.5 [built Mar 12 2018 12:14:52]
UTP: Waiting for device to appear
It is not moving further after below prints.
In kernel I have enabled
CONFIG_FSL_UTP
CONFIG_USB_CONFIGFS_MASS_STORAGE
CONFIG_MASS_STORAGE,
Is there any other macros needs to be enabled in Linux kernel? Whether any changes required in Uboot to be done?
MFG boot log added.
Thanks in advance.
Regards,
Yashavantha
Solved! Go to Solution.
Hi,
Thank you for your support.
MFG tool is working with windows10 OS, but not with windows 7.
Regards,
Yashvantha
Hi Yashavantha
one can try to rebuild mfg tool firmware (files in mfg tool ../firmware folder) with new ones
and using results from ddr test, follow Chapter 4 How to bring up a new MX8M board MX8M_DDR_Tool_User_Guide.docx
i.MX 8M DDR Tool Release
For rebuilding please use sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yashavantha
please try to rebuild mfg tool firmware (files in mfg tool ../firmware folder) with new ones
and using results from ddr test, follow Chapter 4 How to bring up a new MX8M board MX8M_DDR_Tool_User_Guide.docx
i.MX 8M DDR Tool Release
For rebuilding please use sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide
Best regards
igor
Hi Igor,
I am not using the default binaries in firmware folder, I have already build with updated DDR changes and using the same binaries in firmware folder too.
And I'm doing standalone compilation of u-boot and kernel source code, not through yocto.
Thanks and Regards,
Yashavantha
Hi Yashavantha
suggest to try procedure using yocto, as this is nxp officially supported option.
For non-yocto options one can try to get help with Professional Services
Best regards
igor
Hi Igor,
Thank you.
But is there anything can you say after looking at MfgTool.log which I have attached above??
Thanks and Regards,
Yashavantha
Hi,
Thank you for your support.
MFG tool is working with windows10 OS, but not with windows 7.
Regards,
Yashvantha