I.MX233 SDK_V0912 or WCE600_MX23-EVK_10.05.02_SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX233 SDK_V0912 or WCE600_MX23-EVK_10.05.02_SDK

662 Views
rddesign01
Contributor I

I am looking for I.MZ233 SDK_V0912 WCE600_MX23-EVK_10.05.02_SDK_MM.exe. Current have the I.MX233 development board to start working on project which did not come with the SDK to install. NXP support stated I should ask the community for help since they don't support wince anymore. If anyone can point me to the right direction or know how I can get the SDK, I would really appreciate it.

Labels (1)
0 Kudos
Reply
4 Replies

557 Views
rddesign01
Contributor I

Thank you all for all your help. I will try the file.

0 Kudos
Reply

557 Views
rddesign01
Contributor I

Hi, I already created service request and this is the response stated:


Unfortunately we don´t support wince anymore. You will have to ask to community for it.

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.

Best regards,
Alfredo
Technical Support
NXP Semiconductor

----------------------------------------------------------------------------------------------

This message is in reply to the following support case:
Case: 00179815_
Date Opened: 9/19/2018

0 Kudos
Reply

557 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Alfredo is right, nevertheless, You may try files (link), that were sent You directly.

Regards,

Yuri.

0 Kudos
Reply

557 Views
igorpadykov
NXP Employee
NXP Employee

Hi vladimir

please create service request

https://community.nxp.com/docs/DOC-329745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply