You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)
Hello,
Looks like the problem concerns the SDK EVKB release (2.3.1):
“The issue is the EVKB examples include the header information (IVT and FCB),
embedded in the source code (XIP folder). When elftosb runs it encounters code
in an area not expected and it stops.”
The following may be helpful:
https://community.nxp.com/docs/DOC-340156
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
We are using SDK-v2.4.0. and as per the document you have suggested that IVT and FCB header issue will not affect when we use MFGTool to flash the firmware also MFGTool link mentioned in the i.MX RT1050 CMSIS-DAP drag-and-drop programming is not accessible.
Please correct me if my understanding is not proper.
Thanks.