Reference Design for IMXRT 1050.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reference Design for IMXRT 1050.

1,442 Views
manuardi
Contributor II

Hi,

Is there a reference design available for IMXRT 1050 ? The EVK boards schematics are available, which is very helpful, but hopefully a smaller implementation can be done. Are the ext DC/DC for VDD_high_IN (why not LDO ?) and the reset circuits (2 of them) mandatory ? 

Thank's in advance for your reply.

0 Kudos
Reply
1 Reply

853 Views
Yuri
NXP Employee
NXP Employee

Hello,

1.

  The following Web contains recommended i.MX RT1050 designs links:

i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP 

In particular:

i.MX RT1050 Evaluation Kit|NXP 

iMX RT1052 OEM Board | Embedded Artists AB 

2.

  Customers can use own power supply scheme, assuming power supply voltages satisfy

specs and recommended for i.MX RT1050 power up sequence is provided.  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------