Hello.
We need to read unique NFC tag ID by using built-in (on Windows 10 tablet PCs) NXP NFC reader, under Windows 10. Unfortunately, Microsoft don't implemented tags UID support in the Windows.Networking.Proximity namespace (but it's a loooong waiting feature request, since year 2014!).
However, if I can read that tag from regular Win32 app, it will be (at least) a good workaround for us.
NXP NearFieldProximity provider driver on our Windows 10 tablet PCs is listed as \\?\acpi#nxp5442#1#{fb3842cd-9e2a-4f83-8fcc-4b0761139ae9}, and uses following files:
So, my questions are:
This issue is a "showstopper" for us now: without knowing NFC tag UID, we can't prevent tags cloning :smileysad:
I have the same task
in DeviceManager the it shows the NXP dirver dlls:
NxpNfpProvider.dll
FwlibNpc_3x.dll
WUDFRd.sys
Is it possible to get some information/description on the driver dlls, so it would be possible to use it?