Hello Anshul,
I do not think so we have the support for USB Gadget in UBOOT, only basic MSD, and CDC, if you want to test the USB to LAN you need to be with the full Linux Support. and you need to have the driver for the USB stick that you are planning to use.
Hope this helps., Have a happy new year 2018.
Hello Jamesbone,
Thank you for reply. In U-Boot, i am able to find Support for USB Storage device('usb start' command is available),
but i am not able to find the support for Ethernet device via USB(eg: USB to LAN converter).
if any body can help on this that would be helpful for me.
--Anshul