USB to LAN test for IMX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB to LAN test for IMX6UL

635 次查看
anshulkhare
Contributor III

Hi All,

I have an iMX6UL board,
i am doing U-Boot USB to LAN Test .
is there any command to perform the test in U-Boot

any suggestion to perform the test would be appreciated .

Best Regards,

Anshul

标签 (2)
0 项奖励
2 回复数

457 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Anshul,

I do not think so we have the support for USB Gadget in UBOOT,  only basic MSD, and CDC,  if you want to test the USB to LAN you need to be with the full Linux Support. and you need to have the driver for the USB stick that you are planning to use.

Hope this helps.,  Have a happy new year 2018.

0 项奖励

457 次查看
anshulkhare
Contributor III

Hello Jamesbone,

   Thank you for reply. In U-Boot, i am able to find Support for USB Storage device('usb start' command is available),

but i am not able to find the support for Ethernet device via USB(eg: USB to LAN converter).

if any body can help on this that would be helpful for me.

--Anshul

0 项奖励