Voltage Compatibility of DDR3!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage Compatibility of DDR3!

Jump to solution
1,265 Views
qammarabbas
Contributor IV

Hi,

I wanted to ask if pins of DDR3 RAM devices can be directly connected with the pins of T1042 processor. Do we need any device in between them for the purpose of voltage compatibility or will it work fine otherwise? Please let me know about it. Thank you!

Tags (1)
1 Solution
1,112 Views
ufedor
NXP Employee
NXP Employee

You are going wrong direction.

The processor normal operation is guaranteed only when the Data Sheet requirements are fulfilled.

View solution in original post

8 Replies
1,113 Views
ufedor
NXP Employee
NXP Employee

T1042 does not support DDR3 SDRAM.

DDR3L SDRAM pins have to be directly connected to the T1042 SDRAM interface when GVDD=1.35V

0 Kudos
Reply
1,113 Views
qammarabbas
Contributor IV

But the datasheet of DDR3L RAM (8Gb Micron) mentions that its maximum I/O voltage is 1.98V whereas maximum I/O voltage of T1042 is 1.48V. Won't it make them incompatible?

0 Kudos
Reply
1,113 Views
ufedor
NXP Employee
NXP Employee

Why you compare maximum voltages?

The DDR3L should be able to work at 1.35V.

0 Kudos
Reply
1,113 Views
qammarabbas
Contributor IV

I am talking about the I/O pins. DQ pins for instance. If voltage on any of them exceeds beyond 1.48V(maximum that processor's DDR controller pins can accept) won't it harm the processor?

0 Kudos
Reply
1,113 Views
ufedor
NXP Employee
NXP Employee

It definitely will harm.

0 Kudos
Reply
1,113 Views
qammarabbas
Contributor IV

Can you please tell me a harmless way of interfacing SDRAM device with T1042? Thank you!

0 Kudos
Reply
1,113 Views
ufedor
NXP Employee
NXP Employee

You are going wrong direction.

The processor normal operation is guaranteed only when the Data Sheet requirements are fulfilled.

1,113 Views
qammarabbas
Contributor IV

I got it now. Thank you ufedor‌!

0 Kudos
Reply