S32K144 3-Wire SPI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 3-Wire SPI?

2,932 Views
esaias_pech
Contributor I

Hi,

I'm using S32 Design Studio with S32K144 (with the drivers provided by NXP), how can I use 3-wire SPI on the S32K144 in conjunction with the drivers? 

I need to interface with a chip that only provides 3 pins:

* Clock

* Chip Select

* Data Input/Output

Do I need to make any HW Modifications? (e.g. something like this? Interfacing with 3-wire SPI – Total Phase)

Labels (1)
0 Kudos
Reply
5 Replies

2,455 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

This protocol is not supported by LPSPI, so if you need to use it you must implement the circuit from figure 2 (with that resistor).

Best regards,

Razvan

0 Kudos
Reply

2,455 Views
esaias_pech
Contributor I

Hi Razvan, 

Thank you for replying. Based on the datasheet, the protocol should be supported, although it's called "half-duplex" or "single wire" (see screenshots below), by the way, I wish the datasheet had a section on how to use that mode (what registers to modify with what values) instead of searching all over the chapter for "half-duplex" or "single wire".

I'm trying to use the LPSPI driver provided as part of the S32K SDK, but it seems that it's designed with a full-duplex SPI connection in mind. 

I tried the HW modification while calling the LPSPI_DRV_MasterTransferBlocking function but I get whatever was sent on the Rx buffers.

pastedImage_1.png

pastedImage_4.png

0 Kudos
Reply

2,455 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Probably the right therm is LPSPI doesn't have "native support" for 3-wire because the work-flow is totally different.

Now, let's get back to your problem.

Please answer to the following questions:

1. what is the frame size in LPSPI configuration?

2. what is the size of the rx/tx in your 3-wire protocol?

3. How do you call  LPSPI_DRV_MasterTransferBlocking function?

Best regards,

Razvan

0 Kudos
Reply

2,455 Views
esaias_pech
Contributor I

1. I set it up to 8-bit

2. To read from the device: Write 8 bits of register address and then read 8 bits for the value.

3. I tried different ways:

- Sending a TxBuffer and a RxBuffer of 2 bytes each.

- Calling it once to write the address (1 byte) and then calling it again to read the address.

I checked the driver and by default it calls the following function, which means that it's the pins are configured for 2 Data Lines, am I right? 

(void)LPSPI_SetPinConfigMode(base, LPSPI_SDI_IN_SDO_OUT, LPSPI_DATA_OUT_RETAINED, true);

0 Kudos
Reply

2,455 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Please try the following set-up:

Configure the frame size to 16 bit and send with LPSPI_DRV_MasterTransferBlocking  2 bytes.

I suppose that your frame size is 8, so after 8 bits the cs toggle, so your device logic is reset. I think you should keep CS negated during all 16 bits.

Yes, the driver configures the pins for 2 data lines.

Best regards,

Razvan

0 Kudos
Reply