How to do the USB 2.0 HS compliance TEST HOST in WinCE 6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to do the USB 2.0 HS compliance TEST HOST in WinCE 6?

765 Views
jungsookim
Contributor I

Hi

I am developing the Embedded Board with i.MX6 solo in WinCE 6.

For the USB 2.0 HS compliance test of HOST(not otg), I heard that I should implement some code using the USB test mode for generating test packet.

is there recommeded codes or functions for that?

if there is, please let me know.

thanks

0 Kudos
Reply
1 Reply

549 Views
igorpadykov
NXP Employee
NXP Employee

Hi jungsoo

please refer to simple SDK example (sdk/drivers/usb/test/usb0_host_testmodes_test.c)

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply