Cannot export specific gpio pins. How to check what uses GPIO pins?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot export specific gpio pins. How to check what uses GPIO pins?

10,219 Views
Hirotoshi_Sato
Contributor II

Hi,

I use an i.mx6 board and am configuring a device tree.

I changed a dts file and put the dtb file in a boot partition.

I set GPIO4_IO19 in dts file as follows.

&iomuxc {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_hog_1>;
imx6ul-evk {
pinctrl_hog_1: hoggrp-1 {
fsl,pins = <
...
MX6UL_PAD_CSI_VSYNC__GPIO4_IO19 0x0000B0B0
...
>;
};

...

At first MX6UL_PAD_CSI_VSYNC__GPIO4_IO19 was defined in other group (usdhcgrp) but I commented out them.

After booting, I checked if gpio is successfully determined as I set.

The result is 

echo 115 > /sys/class/gpio/export
-sh: echo: write error: Device or resource busy

So I checked this.

cat /sys/kernel/debug/gpio


GPIOs 0-31, platform/209c000.gpio, 209c000.gpio:
gpio-10 (phy-reset ) out lo

GPIOs 32-63, platform/20a0000.gpio, 20a0000.gpio:

GPIOs 64-95, platform/20a4000.gpio, 20a4000.gpio:
gpio-68 (ft5x06_irq_gpio ) in hi

GPIOs 96-127, platform/20a8000.gpio, 20a8000.gpio:
gpio-109 (? ) out lo
gpio-115 (cd ) in lo
gpio-116 (? ) out lo
gpio-117 (? ) out lo
gpio-118 (sysfs ) in hi

GPIOs 128-159, platform/20ac000.gpio, 20ac000.gpio:
gpio-128 (phy-reset ) out lo

gpio-115 is used by cd. What is cd ?

I want to use it as sysfs to read the state. Any other way to read it ? 

Furthermore, gpio-10, 68, 109, 116, 117 is used by other device.

How can I use them by sysfs?

Thank you for your cooperation.

Labels (4)
0 Kudos
Reply
5 Replies

6,019 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

6,019 Views
Hirotoshi_Sato
Contributor II

Hi igor, 

Thank you for your answer.

I am afraid that I have read the link and it would not help me.

(This time the using device is ?, so I cannot find.)

I think dts file is related to this issue 'cause I think only dts file includes pin control, but I couldn't find out.

Would you give me any other adivice?

Best regards,

Hiro

0 Kudos
Reply

6,019 Views
BiyongSUN
NXP Employee
NXP Employee


i.MX Development Miscellanea(i.MX 开发杂记)
https://community.nxp.com/docs/DOC-335198

Accessing GPIO From UserSpace

0 Kudos
Reply

6,019 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hiro

as these are general linux questions, it may be posted

on kernel mail lists.

Majordomo Lists at VGER.KERNEL.ORG 

Best regards
igor

0 Kudos
Reply

6,019 Views
Hirotoshi_Sato
Contributor II

Hi igor, 

Thank you for your replying.

I found my dts file has woding about the gpio.

At first I think gpio is only defined in &iomuxc {...} in dts, but there are other definition in the dts file.

Best regards

0 Kudos
Reply