Unused USB_OTG2_VBUS pin of i.MX6SX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused USB_OTG2_VBUS pin of i.MX6SX

Jump to solution
679 Views
torus1000
Contributor V

Hi,

According to IMX6SXCEC sect.4.2.1 Power-Up Sequence :

  [only] USB_OTG1_VBUS and USB_OTG2_VBUS are not part of the power
  supply sequence and may be powered at any time.

Is it OK to leave USB_OTG2_VBUS pin float if I don't use USB OTG2?

Or I should pulldown with 10k ohm resister?

Can anyone help me?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
578 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes it is ok to leave USB_OTG2_VBUS pin float if one don't use USB OTG2.

It is described in Table 2-17. Recommended connections for unused analog interfaces

IMX6SXHDG Hardware Development Guide for i.MX 6SoloX

http://www.nxp.com/assets/documents/data/en/user-guides/IMX6SXHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
579 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes it is ok to leave USB_OTG2_VBUS pin float if one don't use USB OTG2.

It is described in Table 2-17. Recommended connections for unused analog interfaces

IMX6SXHDG Hardware Development Guide for i.MX 6SoloX

http://www.nxp.com/assets/documents/data/en/user-guides/IMX6SXHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply