Hello Techies,
I am working in CAN FD. I am trying with 500kbps/2Mbps Nominal(arbitration) and data bitrate.
When i am choosing Nominal sampling point : 80 , Data sampling point : 70
Nominal sampling point : 70 , Data sampling point : 65
CAN FD transmission is working.
But when i am choosing same sampling point for both nominal and data bits, then it is not working.
For example Nominal sampling point : 80 , Data sampling point : 80
Nominal sampling point : 70 , Data sampling point : 70
For these settings CAN FD transmission is not working.
Is that anything is not proper in my settings or Is there any logic behind this selection of sample point between
nominal and data fields.
Thanks
Alagappan
Hi pon alagappan,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi jeremyzhou,
Neither i am able to view any code/settings nor able to download software package. Download option in the link you mentioned was disabled.
Thanks
Pon Alagappan M
Hi pon alagappan,
You need to build the SDK manually, the thread illustrate the complete steps.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------