Hi,
I have been working in imx7d sabresd. Right now I am testing SPI interface(in mikrobus - ECSPI3). In board SPI chip select is GPIO6_IO22(address 3033_0228) and i configured it as a chip select from device tree ,and GPIO5_IO9(address 3033_01ac) is configure as a GPIO not as a SS2(chip select) and it is in LOW state. When I am trying to communicate over SPI, because of low state of this pin(GPIO5_IO9) that SPI device also get selected and I am getting wrong data.
I tried by isolating GPIO5_IO9 connection from SPI(through hardware), so it is working fine.
Is this expected behaviour in imx7d?
If I want to do this by software, how can i do?
Million thanks in advance.
Hi DEVEN
on sabre schematic SPF-28590 p.16, TP_ESPI_SS_B is connected by jumper JP1
to TP_SPI_SS_B, had you checked it.
Schematics (2)
Design files for i.MX 7Dual (REV D)
Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 7Dual (REV D)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------