Regarding i.MX7D(19 x 19 mm package) 's Vss(AD05)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding i.MX7D(19 x 19 mm package) 's Vss(AD05)

731 Views
tomohisa_sakamo
Senior Contributor II

Hi Support -Tean,

We have one question regarding datasheet 0f i.MX7D(19 x 19 mm package)'s Vss(AD05).

We would like  to confirm 19 x 19 mm package's datasheet information.
Document:IMX7DCEC.pdf(Rev.4) P140

We can not find AD05(or VSS130).
Latest Rev.4's datasheet or the older is same.
BTW,we can refer AD05(or VSS130) by schematics(i.MX7D Sabre-SDB Rev.d) and Pins Tool(V2.00).

If it is a leak, we would like to be modified when updating the datasheet.

Best Regards,

Labels (2)
0 Kudos
Reply
2 Replies

613 Views
Yuri
NXP Employee
NXP Employee

Hello,

Thanks for this information.

I reported about the doc issue to the team.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply

613 Views
Yuri
NXP Employee
NXP Employee

Hello,

  AD05 will be added to the table 101  in the next release of the document.

Regards,

Yuri.

0 Kudos
Reply