p1022 power on reset problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

p1022 power on reset problem

435 Views
zeevg
Contributor I

Hi,

I working to bring up new board.

I see problem booting from parallel nor.

When making the reset via the ICE the booting is started.

when booting after power up or using reset switch (connected to the input of supervisory) the booting sometime not started.

I drive The CPU HRESET pin from supervisory (which guaranty clean and long signal) to AND gate which inputs are the ICE_Hreset and POReset.

In addition AND gate which inputs are the ICE_TRST and POReset drive the CPU TRST pin.

Pls. advise

Zeev Gerber

0 Kudos
Reply
1 Reply

364 Views
ufedor
NXP Employee
NXP Employee

It is needed to check the processor connection schematics as a whole.

Please create a Technical Case and provide the schematics:

https://community.freescale.com/thread/381898

0 Kudos
Reply