S32 Studio Compile Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Studio Compile Error

2,465 Views
qiaodeng
Contributor II

Hi,

   I encountered the following error when compiling my project using S32:

pastedImage_1.png

What does that mean? How should I handle this?

Regards,

Qiao

Labels (1)
0 Kudos
Reply
5 Replies

2,048 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

error Unsupported relocation against PIR or r4 is caused by incorrect syntax. If you use inline assembler and GPR registers, you have to use following syntax:

asm("e_li  %r0, 0");

There must be character % near the SPR register name.

Hope it helps.

Regards,

Martin

2,048 Views
qiaodeng
Contributor II

Hi Martin,

I've found them and add % , now only the PIR error left. How should I deal with this? Thanks!

pastedImage_1.png

Regards,

Qiao

0 Kudos
Reply

2,048 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I do not know, which microcontroller you use, but PIR register is special purpose register. You have to look to the core reference manual for appropriate core and find the number of the PIR register which you use instead of PIR.

Regards,

Martin

0 Kudos
Reply

2,048 Views
qiaodeng
Contributor II

Hi Martin,

     The MCU is MPC5746R, the code file is from MCAL , I just import  them into my project and don't know why they can not be complied.

Regards,

Qiao

0 Kudos
Reply

2,048 Views
stepank
Contributor I

May be you have swapped operands for this instruction ? It is common error of newbies.

0 Kudos
Reply