Hi,
Thanks for reply.I'm using FRDM-64f board.First I checked my code alone
using the project uart non blocking,with interrupt and which is working
perfect.Then I moved the same code into the lwip tcp echo demo
project,which is now showing some issues.
nRet = UART_DRV_Init(BOARD_DEBUG_UART3_INSTANCE, &uartState,
&uartConfig);
pFunc = (uart_rx_callback_t *)uart_Callback;
UART_DRV_InstallRxCallback(BOARD_DEBUG_UART3_INSTANCE
,(uart_rx_callback_t)pFunc ,&rxChar, 0, NULL);
NVIC_SetPriority(I2C0_IRQn, 3U);
while(true)
{
ReceiveCommandFromSerial();
UART_DRV_ReceiveData(BOARD_DEBUG_UART3_INSTANCE , &rxChar , 8u);
}
}
void uart_Callback()
{
__asm("nop");
}
If I use UART_DRV_SendData() function the whole board is getting hanging.
--
Regards
AJAY K R
Hello Ajay,
Next time please put the replay after your question place .
If you create a new one like this, it is hard to find your reply, thanks!
BR
Alice