Hi all,
I try to figure out which IDE supports programming the above mentioned chip. It is a S12 based relay driver with LIN interface. But i could not find which S12 derivate I should choose in CodeWarrior to get the correct controller.
Greetings
Ralph
IDE:
CodeWarrior v5.1 eval --> 32kB Code Size maximum
Patch:
CodeWarrior for HCS12 v5.1 MM912 x634 ServicePack.exe
This should work ...