Hi, everyone
I'm using NXP’s PTN3460IBS/F1 and there are some problems confused me:
1. I know it supports single bus or dual bus LVDS signaling with color depths of 18 bits per pixel or 24 bits, but I just want to use single LVDS bus.
How should I configure it (The datasheet told me I should pull the CFG1 down)?
Do I need to change other configurations of the hardware and software?
2. Which one should I chose between Odd bus and Even bus when I just want to use single LVDS bus?
Thank you,
Crosper Liu
Hi Crosper,
There is no need to change the configuration for single LVDS bus usage. Odd bus will be selected when CFG1 is set to LOW.
Best regards,
Tomas