PTN3460IBS/F1 configurations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PTN3460IBS/F1 configurations

547件の閲覧回数
crosperliu
Contributor I

Hi, everyone

I'm using NXP’s PTN3460IBS/F1 and there are some problems confused me:

1. I know it supports single bus or dual bus LVDS signaling with color depths of 18 bits per pixel or 24 bits, but I just want to use single LVDS bus.

How should I configure it (The datasheet told me I should pull the CFG1 down)?

Do I need to change other configurations of the hardware and software?

2. Which one should I chose between Odd bus and Even bus when I just want to use single LVDS bus?

Thank you,

Crosper Liu

タグ(1)
0 件の賞賛
1 返信

419件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Crosper,

There is no need to change the configuration for single LVDS bus usage. Odd bus will be selected when CFG1 is set to LOW.

Best regards,

Tomas

0 件の賞賛