Hi,
I have a QorIQ p1025rdb eval board with me. I have taken the sdk 1.2 where the board is supported and have the setup ready, with uboot.
There is an HV in the tmp/deploy/images folder of the yocto release dir. But i could not located the HV DTB, as told in the support document chapter 4.2.1.8 for Hypervisor Deployment.
Does P1025RDB is supported for nxp hypervisor ?
If so could you let me know how to configure the uboot to load the hypervisor and where can i locate the dtb ?
Regards,
Ram
The embedded hypervisor is not supported on P1025 or any other e500v2-based SoC. KVM is supported, though.
Also note that SDK 1.2 is very old. I recommend using a recent upstream kernel instead, especially if you want to use KVM.