MPX5100DP - MAX Pressure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPX5100DP - MAX Pressure

649 Views
nikolaperencevi
Contributor I

Hi, 

in datasheet I find that max difference between P1 and P2 must be 400kPa. Which is max pressure to I bring to P1 and P2?

Can I get 1 MPa at both inputs, on example?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

498 Views
nikolaperencevi
Contributor I

OK, thank you, I will try with 10bar.

0 Kudos
Reply

498 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Nicola,

I do not know this max static pressure. However, 1MPa is OK as long as the difference between P1&P2 is less than 400kPa (and P1>P2).

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply