Dear all,
We have a question about Absolute Maximum Ratings for i.MX6Solo.
We found a difference between Rev5 and Rev6 of Datasheet.
For IMX6SDLCEC Rev. 5, 06/2015,
- VDD_ARM_IN Max value is 1.5V.
- VDD_ARM_CAP Max value is 1.3V.
For IMX6SDLCEC Rev. 6, 08/2016,
- VDD_ARM_IN Max value is 1.6V. (LDO enabled)
- VDD_ARM_CAP Max value is 1.4V. (LDO enabled)
Would you tell me the reason why these values were changed to?
Best Regards,
Yuuki
Hello,
According to section 7 (Revision History) of the Datasheet IMX6SDLCEC Rev. 6, 08/2016 :
"All maximum voltages increased (improved)." This is result of more careful testing.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------