LPC 24xx ISP locked

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 24xx ISP locked

651 Views
michalmatejka
Contributor I

We have LPC 2468 with internal flash and need to reprogramme with our code by ISP. Probleme is, that IC is locked and setted security...Is a way to un-lock device, erase  and burn new code. We use Flash Magic ..

Labels (2)
0 Kudos
Reply
1 Reply

486 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Michal,

You mean the CRP has been implemented? if CRP1/2 is set, you can use FlashMagic to erase the flash.

If CRP3 is set, ISP mode only can be entered by user code.

161426_161426.pngpastedImage_1.png

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply