Is T4240QDS SRIO Internal Loopback Possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is T4240QDS SRIO Internal Loopback Possible?

754 Views
jimccall
Contributor I


Hello,

I'm trying to modify the code in Document AN4972 to create a SRIO Loopback test on a single instead of transmitting it to a secondary board. I was wondering if it was, in fact, possible to even create an internal loopback for SRIO.

I saw the SerDes ports had a register (SerDesx_LNnTCSR3) for each lane of each SerDes controller. I was wondering if this meant that SRIO also could be looped back from TX to RX by enabling this register or if an entire slew of registers needed to be changed.

Thank you!

Labels (1)
0 Kudos
Reply
1 Reply

503 Views
Pavel
NXP Employee
NXP Employee

Look at NXP Community for this problem:

https://community.nxp.com/thread/355957

See also the following page:

http://www.alterawiki.com/wiki/RapidIO_Gen1_Debug_Checklist


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply