Hi,
We are attempting to boot nitrogen6_max board from the eMMC.
It seems we'll have to program certain eFUSE since there is no boot-switch option.
Since these changes are irreversible, I wanted to know if it was safe to program the following fuses with following values? Are these changes sufficient to enable eMMC boot on nitrogen6_max board?
Before
BOOT_CFG[4:0]: 0x00000005: = 0x18000030
After
BOOT_CFG[4:0]: 0x00000005: = 0x18005878
Thanks and Regards,
Anand Mistry