iMX28 Secure Boot Not a gzip file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX28 Secure Boot Not a gzip file

797 Views
bruce_chen
Contributor I

The Imx28 HAB use mfgtool programming and successed. but power-on board get like below error:

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC

PowerPrep start initialize power...

No HAB Events Found!

                     Battery Voltage = 2.82V

Chargeable battery detected but                                 the voltage is too low for battery                                      powered operation.Booting from 5V                                  power source.

LLLLFLCNo HAB Events Found!

FRAC 0x92925552

memory type is DDR2

                   Wait for ddr ready 1power 0x00820616

Frac 0x92925552

start change cpu freq

hbus 0x00000003

cpu 0x00010001

start test memory accress

ddr2 0x40000000

finish simple test

LLLLLLLLLFLCLLJNFUncompressing Linux...

Not a gzip file

-- System halted

The NXP community has same question like below link

iMX28 Secure Boot issues

but has no right result, has some person same to me error?

The Log first line the HAB print   No HAB Events Found! , Why?

I am modify the kernel compress type from gzip to LZMA. the imx28 repeat reboot, like below:

LLLLLLLLLFLCLLJNFUncompressing Linux... done, booting the kernel.

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC

PowerPrep start initialize power...

No HAB Events Found!

                     Battery Voltage = 2.81V

Chargeable battery detected but                                 the voltage is too low for battery                                      powered operation.Booting from 5V                                  power source.

LLLLFLCNo HAB Events Found!

FRAC 0x92925552

memory type is DDR2

                   Wait for ddr ready 1power 0x00820616

Frac 0x92925552

start change cpu freq

hbus 0x00000003

cpu 0x00010001

start test memory accress

ddr2 0x40000000

finish simple test

LLLLLLLLLFLCLLJNFUncompressing Linux... done, booting the kernel.

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC

PowerPrep start initialize power...

No HAB Events Found!

                     Battery Voltage = 2.80V

Chargeable battery detected but                                 the voltage is too low for battery                                      powered operation.Booting from 5V                                  power source.

LLLLFLCNo HAB Events Found!

FRAC 0x92925552

memory type is DDR2

                   Wait for ddr ready 1power 0x00820616

Frac 0x92925552

start change cpu freq

hbus 0x00000003

cpu 0x00010001

start test memory accress

ddr2 0x40000000

finish simple test

LLLLLLLLLFLCLLJNFUncompressing Linux... done, booting the kernel.

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC

PowerPrep start initialize power...

No HAB Events Found!

                     Battery Voltage = 2.80V

Chargeable battery detected but                                 the voltage is too low for battery                                      powered operation.Booting from 5V                                  power source.

LLLLFLCNo HAB Events Found!

FRAC 0x92925552

memory type is DDR2

                   Wait for ddr ready 1power 0x00820616

Frac 0x92925552

start change cpu freq

hbus 0x00000003

cpu 0x00010001

start test memory accress

ddr2 0x40000000

finish simple test

LLLLLLLLLFLCLLJ

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

616 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The problem may be concerned with memory integrity.

Please check memory with a comprehensive test.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply