Content originally posted in LPCWare by philippschrader on Tue Dec 23 15:35:04 MST 2014
Quote:
Dual core debugging through command line GDB isn't really supported, although is do-able.
...
If you want to communicate with redlink server, you need to use telnet to port 3025
Would you happen to have an example for this? I've never used GDB via telnet.
Quote:
But, I have to ask - why do you want to do this when (as you have already said) it works well through the IDE...
This is mostly a question of automation. For past projects we've set up dedicated test machines that autonomously check out the source code, compile it, load it on the target and then run all kinds of tests. We've set the machine up so developers can submit custom GDB scripts with fancy breakpoints, watch points etc. and provide them with backtraces reg dumps etc. when an error occurs.
Also, I'm personally used to using GDB; I'm fairly proficient at using it. It lets me SSH into work and debug everything remotely.