Content originally posted in LPCWare by a.stahl on Thu May 31 06:17:11 MST 2012
Hello!
On a new bunch of our boards with the LPC1111FHN33/101, I get:
Invalid LPC1111/101 Part ID: 0x2516D02B
Known LPC1111/101 ID(s): 0x041E502B, 0x2516902B
03: Failed on chip setup: Ec(01). Invalid, mismatched, or unknown part
I checked the chip on the board and it is correctly labeled as LPC1111F/101.
According to the user manual UM10398 Rev.8 page 43, valid part IDs for the LPC1111FHN/101 are 0x041E502B and 0x2516D02B. The /102 only has 0x041E502B.
The IDs 0x0416502B and 0x2516902B are for the LPC1111FHN/201.
So there seems to be a problem with LPCxpresso.
If so, is there a way (config file or something) to change the "known IDs" ?
For now, I changed the project setting to MCU type LPC1111/102. It works, but it "doesn't feel right"... Afaik the /101 and /102 parts differ only in existence of the power profiles.
Andreas