Content originally posted in LPCWare by Bernhard Hahn on Mon Jun 08 08:33:42 MST 2015
Hello all,
I am playing with the LPC1549 and his QEI. It works so far, but one problem I found:
The Interrupt for position compare.
In the datasheet I read:
Interrupts can be enabled to interrupt when the
compare value is less than, equal to, or greater than the current value of the position
register
So I understand, that an interrupt occurs for each, less, equal and greater.
But there is only a flag in the interrupt register for equal.
Am I blind, or have I understand something wrong?
Thank you in advanced,
Bernhard