Hello Authority, |
Hello Alice,
Thanks for your help. So far I have progressed in linking mqx library code with my application. And now code is downloaded in DRAM memory also executing for there.
Now I am facing one issue here. Whenever I execute __libc_init_array(); instruction. Code crashes there. Do you have any clue regarding this.?
Thanks and Regards,
Prashant Tawde
Hello Prashant,
Sorry for that i know the MQX functions not very clearly , in order to solve the problem sooner ,
i recommend you ask a question on the MQX thread , there will be MQX expert help you about this .
Hope it helps
Alice
Hello Prashant,
- There is document about Migration from Atollic TRUEStudio to Kinetis Design Studio , i recommend you
create one mew project on KDS, then copy the application code to it .
- You might look at the KINETIS120_SC baremetal code that has example of using only the DDR for debugging an application:
\KINETIS_120MHZ_SC\KINETIS_120MHZ_SC\build\iar\lcdc
- Also there are tips you can refer to : K70 Tower System MQX Application in RAM
- There also the DDR memory initialization tool : K70_120 |Kinetis K70 120/150 MHz MCUs|NXP
Hope it helps
Alice
Hello Alice,
It will be really helpful if you attach KINETIS_120MHZ_SC\build\iar\lcdc file here. I am not able to download it from given link.
Regards,
Prashant
Hello Prashant,
Please check the attachment !
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------