FNET stack with CodeWarrior v10.6.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FNET stack with CodeWarrior v10.6.4

868 Views
christopherbois
Contributor I

Hello, I would like to integrate the FNET stack in my program developed on CodeWarrior v10.6.4. Can you help me?

Labels (1)
0 Kudos
Reply
3 Replies

630 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello.

what chip do you work with?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

630 Views
christopherbois
Contributor I

I work with MPC5606E.

0 Kudos
Reply

630 Views
martin_kovar
NXP Employee
NXP Employee

Hi Christopher,

please look at the following application note. This app note shows, how to implement TCP/IP stack and there are also some examples, how to send and receive data using FNET.

http://cache.nxp.com/files/32bit/doc/app_note/AN4577.pdf?fsrch=1&sr=1&pageNum=1

Here you can download source codes:

http://cache.nxp.com/files/32bit/doc/app_note/AN4577SW.zip

Also you can look at this thread:

Problems about receiving ethernet frame on MPC5604E

If you have any other question, please feel free to write me back.

Regards,

Martin

0 Kudos
Reply