Are MMA51xx & MMA52xx accelerometers susceptible to single event upsets? If so, are there any on-board error detection or error correction capabilities?
Hello Dave,
By single event upset what you exactly mean?
Can you elaborate on this a little bit more? May be like what happens to sensor after a shock event?
Have a great day.
David
Single event upsets (SEUs) are radiation-induced errors in microelectronic devices caused by ionizing particles, also commonly referred to as a bit-flip. With the MMA accelerometers, a concern would be if a single "bit-flip" could significantly affect the operation of the sensor. For example, could a bit flip internal to the sensor cause a +/- 480 g device to think is was a +/- 120 g device, resulting in a 120 g acceleration being reported as full scale, which would inadvertently be interpreted as a 480 g acceleration by the processor that is receiving the data from what it thinks is a +/- 480 g device. Some device types are less susceptible to SEUs (e.g. anti-fuse FPGA). I cannot find any information on the MMA51/52 devices that describes their immunity to SEUs.
Best regards,
Dave
Hello Dave,
I apologize for the delay.
Unfortunately, SEU doesn’t apply to MMA5xxx because it was designed using 250nm process and SEU applies only to processes with much smaller geometries (< ~ 180 nm).
In addition, MMA5xxx has 3-bit CRC which is continuously run on the fuse mirror registers. The CRC is guaranteed to detect all single bit errors. The CRC has a hamming distance of 3 so it will also detect up to 3-bit burst (contiguous) errors.
I hope this information will be useful for you.
If I misunderstood your question, feel free to let me know. I will be glad to help.
Have a great day.
David Diaz.
Note: If this post answers your question, please click the Correct Answer button. Thank you!