DDR with ECC support P2020RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR with ECC support P2020RDB

755 Views
vidyasagartata
Contributor II

DDR_ERR_SBE

0 Kudos
Reply
1 Reply

382 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

P2020RDB does not support ECC for its DDR memory. You can see on the P2020RDB schematics that the P2020 DDR controllers ECC byte lane pins (MECC[0:7], MDQS8/MDQS8#) are not connected to any memory chip. Additional DDR-2 memory chip should be connected to this lane in order to keep ECC syndrome byte for each 64-bit of data in the available DDR-2 (4 x16bits) memory.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply