a black trim that outlines my HDMI Display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

a black trim that outlines my HDMI Display

668 Views
rambabugedela
Contributor I

Hi

I have  IMX6dl custom board and I am using 24 inch HDMI(1920X1080@60) display. I made some changes in myandroid/kernel_imx/drivers/video/mxc_hdmi.c for set exact 1920X1080 resolution.Here I attached my mxc_hdmi.c file.

The problem I have, I have a black trim that outlines my HDMI Display. My resolution is set to the correct settings and all, but  why the monitor wont display in a full-screen resolution.

 

any body Help me Plz

Original Attachment has been moved to: mxc_hdmi.c.zip

0 Kudos
Reply
1 Reply

549 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rambabu

could you try Demo images on link

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply