Hi
I have IMX6dl custom board and I am using 24 inch HDMI(1920X1080@60) display. I made some changes in myandroid/kernel_imx/drivers/video/mxc_hdmi.c for set exact 1920X1080 resolution.Here I attached my mxc_hdmi.c file.
The problem I have, I have a black trim that outlines my HDMI Display. My resolution is set to the correct settings and all, but why the monitor wont display in a full-screen resolution.
any body Help me Plz
Original Attachment has been moved to: mxc_hdmi.c.zip
Hi Rambabu
could you try Demo images on link
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------