I need to integrated a pressure sensor into a pressurised vessel used in microfluidic applications. This vessel will be pressurised with air and with water.
Hello Joseph,
We can only warranty that the pressure sensor will work as long as the internal die of the sensor is not in direct contact with the water.
Other media than dry clean air has the potential to dissolve, or be absorbed by the gel and corrupt the die surface or lead to wire-bond breakage.
You may find more information here.
Please review the following recommendations based on your request:
These families (MPXH6300A and MPXH6400A) of pressure sensors offers high reliability of on-chip integration in a small form factor, targeting automotive and industrial applications.
In regard with the package option, MPXH6300A and MPXH6400A series, are available in super small outline package:
Please find more information and useful documentation at:
Please let me know if this recommendation is useful for you.
If I misunderstood your question, feel free to let me know. I will be glad to help.
Have a great day.
David Diaz.
Note: If this post answers your question, please click the Correct Answer button. Thank you!