I have a small project I am working on and have been moving back and forth between a couple of different PCs, today I noticed that any breakpoints I set in interrupt routines are not detected.
Breakpoints in main and other files are fine.
Have I got a setting wrong somewhere?
I am using KDSK 1.3, PE and FRDM-K64.
OK, this is what I found, after moving from one pc to another, unless I actually edit a file, i.e. events.c, breakpoints do not work in it. If I edit the file and recompile then breakpoints do work.
Is there a way to force a full recompile/make of all files?
OK, just fired up the PC at home and the break points in interrupts are working fine, so it is only a problem on my PC at work.
Do you think it a setting issue in KDS, or a path issue because I am moving the project between computers?
Hi Ernes,
check the breakpoints view: on Kinetis K you can set a 4 hardware breakpoints only (see as well Software and Hardware Breakpoints | MCU on Eclipse ): the breakpoints which are set have a 'checked' mark in the breakpoint view.
Erich
I'm back in the office tomorrow and will try again on the PC there and report back.
I was only setting a single break point so the quantity was not the issue.
Hello Ernest,
If your project now can work well , there is no issue about the path.
And sometimes maybe set more breakpoint for it can not work well .
Anyway , it can work well now.
BR
Alice