Does i.MX6DQ VPU support 4:0:0 (Monochrome) for h.264 high profile?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6DQ VPU support 4:0:0 (Monochrome) for h.264 high profile?

Jump to solution
721 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ VPU.

Please see Table 69-1 in IMX6DQRM Rev.3.

It says h.264 decoder supports HP (High Profile).

According to "Feature support in particular profiles" table in the following site, high profile supports "4:0:0 (Monochrome)".

https://en.wikipedia.org/wiki/H.264/MPEG-4_AVC

Then, do i.MX6DQ VPU and Linux BSP (L3.14.xxx) support "4:0:0 (Monochrome)"?

Best Regards,

Satoshi Shimoda

Labels (5)
Tags (3)
0 Kudos
Reply
1 Solution
641 Views
art
NXP Employee
NXP Employee

Yes, the i.MX6DQ VPU decoder can support Monochrome format in the H.264 High Profile stream. However, the decoder's output format is always 4:2:0 for all profiles/codecs. In case of Monochrome stream, a fake (zeroized) color components will be output.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
642 Views
art
NXP Employee
NXP Employee

Yes, the i.MX6DQ VPU decoder can support Monochrome format in the H.264 High Profile stream. However, the decoder's output format is always 4:2:0 for all profiles/codecs. In case of Monochrome stream, a fake (zeroized) color components will be output.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply